File Locations (Default)
Geo SCADA Expert installs files in several locations. Some of these files you may need to access during the configuration of your system and so you should familiarize yourself with the default locations.
The following section details the default file locations for Geo SCADA Expert on any of the supported Windows platforms:
These are the default file locations—the files on your system may be in different locations, depending on how the system has been installed and configured.
If you cannot locate a file at the default location, check the file's location using the Server Administration Tool, or use the Search facility in Windows.
You can change the location of the server files by using the Server Administration Tool.
You can change the location of log files by using the Move Log Files wizard
Virtual ViewX
The following section details the default file locations for Virtual ViewX server on any of the supported Windows platforms:
- Windows 64-bit File Locations – Virtual ViewX Server.
(Virtual ViewX server is not supported on Windows 8.1.)