Operational Limitations - Client
Geo SCADA Expert has a number of recommended operational limits. Expansion beyond the recommended limits is possible, but may result in a system that is unstable and unreliable. The recommended operational limits for Geo SCADA Expert clients are:
|
Parameter |
Limit |
Notes |
|---|---|---|
|
Minimum ViewX to Geo SCADA Expert server link bandwidth |
2 Mbit |
Exceeding these limits will cause slow performance in ViewX. |
|
Maximum ViewX to Geo SCADA Expert server link latency |
50 ms |
Exceeding these limits will cause slow performance in ViewX. |
|
Minimum Virtual ViewX client to Virtual ViewX server link bandwidth |
1 Mbit |
|
| Minimum Original WebX client to Geo SCADA Expert server link bandwidth |
2 Mbit |
While these are recommended operational limits, we do not guarantee performance even if your system is operating at or under these limits. This is because it is possible to configure aspects such as data processing and client displays that are detrimental to performance. We recommend that you review the Design Guidelines and Performance Guidelines online on the Schneider Electric Community website.
You are restricted to having up to a maximum of 5 Geo SCADA Expert displays open simultaneously on a Virtual ViewX client (providing that your User Account provides
Further Information
Server operational limitations: see Operational Limitations - Geo SCADA Expert Server.