Your First 'Live' Configuration

Your Geo SCADA Expert system can connect to, and interact with, a wide variety of outstations, PLCs, controllers and similar devices. These devices contain 'live' data that is reported to, or retrieved by Geo SCADA Expert and stored in corresponding items in the database. Similarly, Geo SCADA Expert can send controls to the device.

You are now going to configure Geo SCADA Expert to communicate with a hardware device—a SCADAPack Modbus controller that has:

While we recommend that you use a SCADAPack Modbus controller (available from your Geo SCADA Expert agent), you can complete this section without any hardware. However, if you don’t have a SCADAPack Modbus controller, you won’t have live I/O to work with, so to achieve different values and states, you will need to perform Hand Controls on your points.

You need to have the Advanced Modbus driver installed on your system (see Installing ClearCADA).

As you set up your first 'live' configuration, you will learn how to configure the main elements required to operate your system. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

At the end of this section, you can see how much you have learned by accepting our challenge to Test Your Knowledge on 'Live' Configuration.


Disclaimer

Geo SCADA Expert 2022