Configure the General TBox Digital Point Properties

Use the fields at the top of the Digital Point tab to Configure Common Point Properties. Fields that are specific to TBox Digital points are explained below.

  • Number of Bits: Use this combo box to specify the number of bits for the point. This corresponds to the number of consecutive 1-bit points that form the point.

    The number of bits directly affects the number of point states. For further information, see Single and Multi-Bit Digital Points in the Geo SCADA Expert Guide to Core Point Configuration.

  • Format: Specify the format in which the point’s value appears in other ViewX displays, such as Lists (see Define the Format of a Digital Point’s Values in the Geo SCADA Expert Guide to Core Point Configuration).

  • Disclaimer

    Geo SCADA Expert 2022