Totalflow Digital Point

You can use a Totalflow Digital Point object to read and write (control) any value from a Totalflow that is specified by a App/Array/Register that holds a numeric value. For a list of the numeric formats that are supported, see the table in the topic about the Totalflow Numeric Point.

With a Totalflow Digital Point, the driver converts the numeric value that is read from the Totalflow into a digital value in Geo SCADA Expert, allowing for presentation of the data in a digital format. Depending on the type of value, the driver reads and converts the entire value that it reads from the Totalflow into a digital value, or extracts and converts up to three bits of data from the numeric value.

For more information about the Totalflow Digitial Point, see the following topics:


Disclaimer

Geo SCADA Expert 2022