Totalflow Scanner

The Totalflow Scanner database item provides you with the link between Totalflow points and the Geo SCADA Expert server. The configuration of a Scanner allows you to control everything from whether to set the clock in the Totalflow, to the scan rate for attached points.

As part of the requirements for a Totalflow Scanner to be active, you require at least one Totalflow Channel to be configured and enabled (see Totalflow Channel). The Scanner item itself is referenced by Totalflow Point objects.

For information about the object’s configuration and setup, see the following sections:


Disclaimer

Geo SCADA Expert 2022