Supported FontStyle Identifier and Integer Values
            You can include any of several FontStyle identifiers in a TrendSpec definition, in order to specify different font style(s) to the ViewX defaults. In each case, you can specify the required font style using one of these integer or identifier values:
Supported Identifier Values
FontStyleRegular
FontStyleBold
FontStyleItalic
FontStyleBoldItalic
FontStyleUnderline
FontStyleStrikeout
Example:
TitleFontStyle = FontStyleUnderline
Identifier values are case insensitive and cannot include any character spaces.
Supported Integer Values
0 (equating to FontStyleRegular)
1 (equating to FontStyleBold)
2 (equating to FontStyleItalic)
3 (equating to FontStyleBoldItalic)
4 (equating to FontStyleUnderline)
8 (equating to FontStyleStrikeout)
To specify a combination of the above styles, specify the sum of the integers that, when combined, provide the required style.
Example:
LabelFontStyle = 3
(for the font assigned to the y-axis label’s text to appear in bold italic (providing that the font assigned to the LabelFont identifier supports such a style))
LabelFontStyle = 7
(with 7 being the sum of the separate integer values 3 + 4 (that is, FontStyleBoldItalic AND FontStyleUnderline), or 1 + 2 + 4 (FontStyleBold AND FontStyleItalic AND FontStyleUnderline))
For a more detailed example that demonstrates how the various FontStyle identifiers might be defined, see Use TrendSpec to Define an Ad Hoc Trend’s Text Attributes.