TRACE Mandatory Values
            The TRACE section within a TrendSpec definition has to contain two mandatory values: <Data Mode> and <Y-Axis Name>.
You should specify the <Data Mode> before the <Y-Axis Name> and separate the two entries with a comma.
| TRACE Mandatory Values | ||
|---|---|---|
| 
                                 Mandatory Value  | 
                            
                                 Type  | 
                            Comments | 
| 
                                 <Data Mode>  | 
                            
                                 Identifier value  | 
                            
                                 Use to define the type of data that the trace displays. Specify one of these values: Current, RawHistoric, or ProcessedHistoric (For information about the type of data that each option represents, see Add a Trace to a Trend.) Example: Current Only specify an option other than Current if Historic is enabled for the database item that is the source of the trace (for points, Defining Historic Details for a Point; for accumulators, Tabs on Accumulator Forms). A Trace can only have multiple sources if an option other than RawHistoric is specified (see Multiple Source Traces). The <Data Mode> mandatory value is trace independent. As such, the traces on a multiple-trace ad hoc Trend can be assigned different <Data Mode> values to each other.  | 
                        
| 
                                 <Y-Axis Name>  | 
                            
                                 String  | 
                            
                                 Use to identify the y-axis that is associated with the trace. The <Y-Axis Name> is used internally within the TrendSpec definition to link a trace to its respective y-axis. As such, the <Y-Axis Name> in the TRACE section of a definition has to be identical to the <Y-Axis Name> in the corresponding YAXIS section (see YAXIS Mandatory Value). Example: ‘Sensor Value’  | 
                        
If required, you can specify one or more TRACE Optional Values after the above mandatory values in a TrendSpec definition.