XAXIS Mandatory Value
            The XAXIS section in a TrendSpec definition has to have one mandatory value, <X-Axis Mode>.
| Mandatory Value | Type | XAXIS Mandatory Values | 
|---|---|---|
| Comments | ||
| 
                                 <X-Axis Mode>  | 
                            
                                 Identifier value  | 
                            
                                 Use to define the type of time scale used for the x-axis. Specify one of these values: Absolute, RelativeNow, or RelativeLatest. (For information on each type of x-axis mode, see Configure the X-Axis.) 
                                        Example:
                                     
                                    RelativeLatest  | 
                        
If required, you can specify one or more XAXIS Optional Values after the above mandatory value.