Delete a Link or Folder from your Favorites List

You can delete a link or folder from your Favorites List if it is no longer required.

If you delete a folder, the contents of that folder will also be deleted.

To delete a link or folder, either:

  1. Right-click on the link or folder.
    A context sensitive menu is displayed.
  2. Select the Delete option.
    The link or folder is removed from the Favorites List.

Or:

  1. Use the Organize Favorites window to delete the link (see Use the Organize Favorites Window to Organize your Favorites List).

Or:

  1. Select the obsolete link or folder in your Favorites List.
  2. Press the Delete key on the keyboard.
    A message is displayed, asking you to confirm whether you want to delete the selected item.
  3. Select the Yes button to confirm the request.
    The link or folder is deleted from your Favorites List.

Disclaimer

Geo SCADA Expert 2022