Disable Alarms

Associated with: Any item for which an alarm can be raised

Security permission required to access this option: Disable Alarms

The Disable Alarms option on the Object Menu is only available on database items that can have alarms. Access to the option is also dependent on the server configuration (which might restrict access to the option).

The Disable Alarms option allows you to disable (hide) alarms for the selected item.

Select the option on an individual database item, such as a point, to disable the alarms on that item.

Select the option on a Group or Group Instance to disable the alarms on the items in that Group or Group Instance (and in any subgroups insee Disable Alarms that Group or Group Instance).

For more information, see Disable Alarms.


Disclaimer

Geo SCADA Expert 2022