Document Display Area

The ViewX document display area is the main part of the ViewX interface and is where the ViewX displays are shown. These include:

Typically, you will perform many of your tasks from Mimics, Trends, and Lists that are shown in the ViewX document display area.


You can change the size of the ViewX document display area by selecting the left-hand side or bottom boundary and dragging it. This either increases or decreases the height or width of the ViewX document display area—the Explorer Bar and Alarm Banner are resized accordingly. (Your user account permissions may not allow resizing of the Alarm Banner.)


Disclaimer

Geo SCADA Expert 2022