Position

Associated with: All items

This status attribute indicates an item's geographical location in the form of coordinates. Additional information, such as the item's altitude might also be displayed, depending on the item's configuration (see Use the Location Tab to Specify an Item's Geographic Coordinates).

The status attribute is only included on the item's Status display if the item's Position string is populated, or its Location Source is set to be dynamic or inherited from an item that itself has a populated dynamic, static, or inherited Position.

 

52.4068°, 1.5197°

(Coordinates showing latitude, followed by longitude.)


Disclaimer

Geo SCADA Expert 2022