System Security
Geo SCADA Expert security helps to protect the
As a system user, you will be assigned access permissions according to the functions you need to perform, and you will only be able to see the functions that this makes available to you.
You will use a ViewX or Virtual ViewX client that has been configured by a higher level user, which will provide access to the displays and features that you need to carry out your tasks, such as performing actions on database items
System security allows you to manage access to the client. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
When you log off from ViewX, the current settings for the following interface components are stored locally as a client setting and associated with your user account.
These settings are then restored when you log on to the same computer.