Configuring a WITS Firmware Image

Field Device manufacturers may produce firmware updates, which can enhance your WITS Field Device. For example, a firmware update may provide additional functionality.

 

To apply a firmware update to a Field Device, you can:

 

To use Geo SCADA Expert to store and download firmware update files to your Field Devices, you need to create a WITS Firmware Image items:

  1. Log on to ViewX via a user account that has the Configure permission.
  2. Right-click on the System item or a Group item and select Create New and then select DNP3 and then select WITS and then select WITS Firmware Image. This creates a new WITS Firmware Image item. Enter a suitable name for the item.

    WITS Firmware Image items only have configuration settings that are common to many types of database item. These include Identification settings and User Methods settings. These are optional settings.

    If you want to configure the Identification and User Methods settings, use the Form for the Firmware Image item (see Display a Form). For details on the settings:

 

You have now created the WITS Firmware Image item. You will now need to:

You will then be able to:


Disclaimer

Geo SCADA Expert 2022