Is Geo SCADA Expert WITS Verified?
Yes, Geo SCADA Expert (formerly ClearSCADA) versions 71 and above are WITS verified for WITS version 1.1. Geo SCADA Expert also supports WITS versions 1.0, 1.2, 1.3, and 3.0, but is not WITS verified for these versions. The WITS verification means that Geo SCADA Expert has passed an extensive range of tests set by the WITS Protocol Standards Association. The tests were conducted with three other WITS Field Device manufacturers.