Off Scan (WITS Outstation)

Associated with: WITS Outstations

Security permission required to access this pick action: Off/On Scan

The ability to place points and outstations Off Scan is disabled on most systems by default. (Its permission is typically denied on a per server basis.)

WARNING

UNEXPECTED BEHAVIOR OF APPLICATION

Use the Off Scan pick action on an Outstation with care—always check the Field Device’s current activity before deciding whether to use this action. Using the Off Scan action will mean that the Field Device will not log data or generate DNP3 events for all points. For this reason, you need to be certain that other users do not require the Field Device's point data before you put the Field Device Off Scan.

To check whether a Field Device is currently processing a request, look at its entry in the Current Request column of the Outstations List. You can also check a Field Device’s current activity via other displays, for example, the Outstation’s View Status window.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

You can use the Off Scan action to set a Field Device that is currently 'on scan' to 'off scan'. When a Field Device is 'off scan':

Typically, you would set an Outstation to Off Scan when you expect its points to generate unnecessary alarms and/or events, for example, during maintenance.

The current scanning state of a Field Device is shown in the View Status window for the WITS Outstation item

NOTE: The On Scan/Off Scan settings for points are independent of the Field Device's On Scan/Off Scan setting. However, both On Scan/Off Scan settings affect the scanning state for an individual point.

The scanning state of each point is a combination of its individual setting and the Field Device's OnScan/Off Scan setting. If either (or both) is Off Scan, the point is Off Scan. A point is only On Scan if both the Field Device and the point are On Scan.


Disclaimer

Geo SCADA Expert 2022