Status

Associated with: WITS Application programs.

 

The Status attribute shows the status of an application program that is running in the Field Device.

 

The possible status options are as follows:

 

When the status of an application program changes, Geo SCADA Expert may log an event. This event logging is configurable (see Configuring a WITS Application Program)).

The possible status events are as follows:

 

Further Information

Last Updated.

Quality.

Initialize.

Start

Stop

Pause

Resume

Download Configuration (WITS Application Program)


Disclaimer

Geo SCADA Expert 2022