Upload Configuration (WITS Outstation)

Associated with: WITS Outstations.

Security permission required to access this pick action: Configure.

NOTICE

LOSS OF CONFIGURATION CHANGES

If you choose to upload All Configuration, the uploaded configuration will overwrite any existing configuration for the Outstation in Geo SCADA Expert. For this reason, take care when specifying the Upload Mode, as you may lose configuration settings you have applied in Geo SCADA Expert (but have not been downloaded to the Field Device).
Failure to follow these instructions can result in loss of configuration changes.

You can use the Upload Configuration pick action to upload a WITS Field Device's configuration into Geo SCADA Expert. This is only available if your Field Device supports configuration upload (defined in the Device Profile for your Field Device, see Display a WITS Device Profile). Typically, you will only use the Upload Configuration pick action if uploading is part of your chosen configuration strategy (see WITS Configuration Strategies)

If a user changes the Field Device's configuration locally, the Field Device sets a flag to alert Geo SCADA Expert users to the change. For more information, see Local Configuration

If you are going to upload the configuration, and the Outstation or any of its points or profiles are in a Group Instance, you need to be aware of:

  • Property Overrides

    If the necessary Property Overrides are not defined, Geo SCADA Expert will be unable to write the changes to the database and the upload process will be unsuccessful. For more details, see Property Overrides.

  • The Point Conversion Process

    As part of the upload process, Geo SCADA Expert may need to change the type of existing points in the Geo SCADA Expert database. For example, it may convert an Analog Input into a Minimum point so that it matches the configuration being uploaded. This conversion cannot take place if the point is in a Group Instance, as its type is determined by the matching point in the Group Template. For more details, see Importing/Uploading Configuration - Point Conversion.

If an import fails as a result of missing Property Overrides or point conversions being required, Geo SCADA Expert lists the configuration errors in a configuration report (see Configuration Reports for WITS Field Devices). There are no changes made to the Geo SCADA Expert database.

When you select the Upload Configuration action, the Upload Configuration window is displayed.

Upload Configuration - WITS Outstation

The window contains the following fields:

Upload

Select which parts of the configuration you want to upload. The options are:

All Configuration

Select this option if you want Geo SCADA Expert to upload the complete configuration of the Field Device, including the bulk configuration file, a matching incremental configuration file, and application programs.

Typically, you would only select All Configuration if a mistake has been made with the versions of the bulk configuration file or application program files. For example, if the bulk configuration has been modified without changing the version. Using this option allows you to force an upload so that both Geo SCADA Expert and the Field Device have the same configuration.

Changed Configuration

Select this option if you only want Geo SCADA Expert to upload any part of the configuration that does not exist in the Geo SCADA Expert database. This includes the incremental configuration. However, it will only include the bulk configuration file or application programs if they have a different version to those in Geo SCADA Expert.

Use this option if the file versions are correct, as it is an efficient way of uploading configuration.

From WITS Version 1.2 or later: When a user changes the Field Device's incremental configuration, the Field Device sets a flag to indicate this configuration has changed. Geo SCADA Expert uses the flag to determine if it needs to upload the incremental configuration.

Mode

Select how the configuration upload should overwrite existing configuration changes (for the WITS Outstation and its points and profiles) in the Geo SCADA Expert database. The options are:

Merge

Select this option if you want Geo SCADA Expert to preserve any changes that you have already made to the configuration in Geo SCADA Expert. When Geo SCADA Expert merges the new uploaded configuration with the current configuration in the database, it only updates those incremental configuration records that have not already been modified. If any part of a record has already changed in Geo SCADA Expert, the entire new record will be discarded and the existing changes preserved. For details on the incremental configuration records, see Incremental Configuration File - Content and Syntax.

 

You upload the initial configuration for a Field Device into Geo SCADA Expert and then change an alarm limit for an analog point in the Geo SCADA Expert database.

When you initiate the next configuration upload and select Merge, Geo SCADA Expert will detect that the alarm limit has been modified. It will upload every incremental configuration record except the record for the alarm limit that you changed.

Replace

Select this option if you want the configuration upload to overwrite the entire configuration that is already in place for the Outstation, its points and its profiles.

If the upload includes configuration that does not exist in Geo SCADA Expert, Geo SCADA Expert creates the appropriate items and configuration automatically. If the configuration already exists in the Geo SCADA Expert database, Geo SCADA Expert just updates the configuration settings to match those of the upload. This applies to both Merge and Replace.

WITS Files Only

Select this option if you only want to upload the bulk configuration and incremental configuration files into the database. When you select this option and upload the configuration, Geo SCADA Expert does not create any new points or overwrite the existing configuration of the points or profiles. The existing configuration of the points or profiles within the Geo SCADA Expert database, typically inherited from a Group Template will remain the same. However, any existing points or profiles in the Geo SCADA Expert database, that do not exist in the uploaded configuration will become invalid (this is by design, to help prevent them from being downloaded in future).

When you select the OK button, Geo SCADA Expert begins the upload process. If the Mode is set to Merge or Replace, it replaces the existing configuration for the Outstation item, its points and its profiles, with the configuration in the uploaded incremental configuration file. It may also upload the bulk configuration file and application program files, if they have different versions or you chose to upload all configuration. If the Mode is set to WITS Files Only, it does not create any new points or profiles, or overwrite the existing configuration. However, any points or profiles that exist in the Geo SCADA Expert database but not in the uploaded configuration will become invalid.

If the upload process is unsuccessful, no changes are made to the configuration and an error report is generated. The report indicates the reasons for the upload failure (see Configuration Reports for WITS Field Devices).

If Geo SCADA Expert uploads a bulk configuration file, it will store the file in the database. This will overwrite any existing bulk configuration file that was already stored in the database (for the Field Device).

If Geo SCADA Expert uploads new application program files, it creates new Application Program items in which to store them.

Any application programs that have been deleted locally in the Field Device, but exist in the Geo SCADA Expert database, will be taken out of service. This is designed to help to prevent them from being downloaded in future. Geo SCADA Expert changes the status of the application programs to indicate that they do not exist in the Field Device and also raises an alarm ('Application deleted from Outstation'). If the Application Program is in a Group Instance, it will only be taken out of service if it has a Property Override in place for the In Service property (see Property Overrides).

If you upload configuration into items in a Group Instance (the Outstation or any of its points, profiles or application programs), Geo SCADA Expert has to determine which configuration to use. It compares the uploaded configuration settings to those that are already in place in the Geo SCADA Expert database, on a field-by-field basis. If the upload configuration settings are different to those in Geo SCADA Expert, Geo SCADA Expert checks if the required Property Overrides are defined. If they are, the upload configuration overwrites the existing configuration. Any settings that are the same as those in Geo SCADA Expert are discarded. If the upload contains points, profiles and application programs that do not exist in Geo SCADA Expert, new items are created to store the configuration. These new items are created automatically.


Disclaimer

Geo SCADA Expert 2022