Vendor Name

Associated with: WITS Device Profile.

 

The Vendor Name attribute shows the name of the organization that manufactures the device type to which the device profile relates. The Vendor Name is a maximum of 8 characters in length and is usually in upper case.

Example:

SCHNEIDR

You can find the Vendor Name in the Device Identification section of the device profile ((see Display a WITS Device Profile)). The name is also registered with the WITS Protocol Standards Association (for more information, see http://www.witsprotocol.org).

A Field Device has a set of DNP3 device attributes that Geo SCADA Expert reads whenever it establishes communications with the device. The Manufacturers Name String (ID:252) attribute should match the Vendor Name attribute in the device profile. If the names do not match, it might mean that you are using the wrong device profile.


Disclaimer

Geo SCADA Expert 2022