Configure a WITS Field Device to Listen and Initiate via the Same Connection

If you want your WITS Field Device to be able to initiate network connections with Geo SCADA Expert, and wait for connections made by Geo SCADA Expert, you can:

Some WITS Field Devices support Dual End Points, which means they can both initiate and listen on a single network connection. (If a Field Device can 'listen', it means it can wait for Geo SCADA Expert to initiate a network connection. Similarly, Geo SCADA Expert can 'listen' for the Field Device to initiate a network connection).

When permanent communications are used, and the End Points are Dual, Geo SCADA Expert and the Field Device will attempt to initiate a connection on startup. They will attempt to initiate a connection repeatedly until one of them makes a successful connection.

If on-demand communications are used, and the End Points are Dual, both Geo SCADA Expert and the Field Device can initiate a connection at any time.

This functionality is dependent on your WITS Field Device supporting network communications.

To configure a WITS Field Device to be able to 'listen' and initiate a network connection:

  1. Log on to ViewX via a user account that has the Configure permission, and then display the Form for the Outstation that represents your Field Device (see Display a Form).
  2. Select the Network tab.
  3. Use the following settings (at the top of the Network tab) to configure the outbound network connection (connection from Geo SCADA Expert to the Field Device):
    • Network—Choose whether a single network or dual network is used. If you choose Dual Network (for network redundancy), you will need to specify the other network settings for Network A and Network B.
    • Host Address—Specify the IP address (or domain name) of your Field Device. Geo SCADA Expert will use this address and the Port number to initiate a network connection with your Field Device.
    • Port—Specify the number of the TCP/IP port on which your Field Device is 'listening'.
    • Device Port—Choose the network communications port that your Field Device uses when 'listening' for connections from Geo SCADA Expert. The network communications port is in your Field Device.

      The ports available in the Device Port setting are taken from the Device Profile (see WITS Device Profiles). The options vary depending on whether the Field Device has a permanent or on-demand connection. For example, if you connected a Schneider Electric Talus T4e to Geo SCADA Expert via an Ethernet cable attached to its E1 port, you would choose the Ethernet 1 option.

    • TCP/IP Type—Choose the protocol that your Field Device uses for communications via the specified Device Port.The protocols that are available for the specified Device Port are defined by the Device Profile (see WITS Device Profiles).
    • End Point—Choose Dual. This configures the Field Device so that it can 'listen' for Geo SCADA Expert to initiate the network connection or can initiate the network connection itself. However, the End Point for the incoming connection also has to be set to have a Dual End Point.

    If your Field Device is behind a router, you may need to configure Geo SCADA Expert to connect to the router (rather than the Field Device). The router will then need to be configured to forward the connection to the Field Device.

  4. Use the settings in the Inbound Connections section to specify the network connection that will be used to contact Geo SCADA Expert:

    Each inbound network connection with End Point: Dual has to have a matching outbound connection (the End Point, Device Port, and TCP/IP Type need to be the same, as they define either end of a single connection). However, this does not mean you are limited to one inbound 'Dual' connection - an outbound connection with End Point: Dual can be shared by multiple inbound connections with End Point: Dual.

    • Host Address—Specify the IP address (or domain name) of the Geo SCADA Expert server. Your Field Device will use this address and the Port number to initiate a network connection with Geo SCADA Expert.
    • Port—Specify the number of the TCP/IP port on which Geo SCADA Expert is 'listening' (see Configure a Channel's Network Connection Properties).
    • Device Port—Choose the network communications port that your Field Device uses when initiating a connection to Geo SCADA Expert. The network communications port is in your Field Device.

      The ports available in the Device Port setting are taken from the Device Profile (see WITS Device Profiles). The options vary depending on whether the Field Device has a permanent or on-demand connection. For example, if you connected a Schneider Electric Talus T4e to Geo SCADA Expert via an Ethernet cable attached to its E1 port, you would choose the Ethernet 1 option.

    • TCP/IP Type—Choose the protocol that your Field Device uses for communications via the specified Device Port.The protocols that are available for the specified Device Port are defined by the Device Profile (see WITS Device Profiles).
    • End Point—Choose Dual. This configures the Field Device so that it can 'listen' for Geo SCADA Expert to initiate the network connection or can initiate the network connection itself. However, the End Point for the outbound connection also has to be set to have a Dual End Point.

    If the Geo SCADA Expert server is behind a router, you may need to configure the Field Device to connect to the router (rather than the Geo SCADA Expert server). The router will then need to be configured to forward the connection to the Geo SCADA Expert server.

  5. Repeat steps 3 and 4 if required:

    Repeat step 3 (for Network B) if a dual network is being used.

    Repeat step 4 for each Geo SCADA Expert server, or if you want multiple connections to the same Geo SCADA Expert server.

    For example, if your Field Device connects to a Hot-Standby Pair, configure one Outgoing connection and two incoming connections, with each of the connections having a Dual End Point. In this scenario, both Server A and Server B use separate inbound connections, but they share a single outbound connection. The outbound connection defines half of the connection between the Field Device and Server A (with the inbound connection for Server A defining the other half). The same outbound connection also defines half of the connection between the Field Device and Server B (with the inbound connection for Server B defining the other half).

    Example: Network Connections with Dual End Point (Hot Standby Pair)

  6. Save the configuration.
  7. Download the configuration to the Field Device by using the Outstation item's Download Configuration (WITS Outstation) action. If your Field Device does not support configuration download, you will need to configure the network settings using the device's Configuration Application.

Further Information

For more details on the common Network settings (Network, Host Address and Port), see Define an Outstation's Network Properties.


Disclaimer

Geo SCADA Expert 2022