WITS-Specific Actions and Methods
This driver is an extension driver. As such, it supports a combination of the pick actions that are supported by its 'parent' driver, in addition to its own driver-specific pick actions. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the pick actions that are supported by this extension driver.
The topics in this section explain the actions that are WITS-specific. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
Further Information
Actions supported by this driver's parent driver: see Using DNP3 Specific Actions.