What is the Syntax for the Field Device Configuration Filenames?

The WITS standard requires the following syntax to be used for bulk configuration filenames:

<name>_<version>.<extension>

The same syntax is also used for application program files.

The WITS standard does not specify a syntax for incremental configuration filenames. We recommend that you allocate the same name to the bulk configuration file and the matching incremental configuration file, and use different extensions for each.

For more details,see:

Bulk Configuration File - Content and Syntax

Incremental Configuration File - Content and Syntax


Disclaimer

Geo SCADA Expert 2022