Specify which File Types can be Downloaded from Virtual ViewX
Use the registry key DownloadFileTypes to configure a collection of permitted file types. The registry key defines which types of file users can download from the Virtual ViewX server. The registry key does not exist by default.
potential for malicious use
To specify the permitted file types:
- On the Virtual ViewX server machine, Access and Run a Registry Editor.
- If it does not exist already, create a new registry key
DownloadFileTypesin Computer\HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\Virtual ViewX.Virtual ViewX enables the external download capability of the specified file types for all users on the server on which the registry key is created.
-
Double-click the registry key to add further permitted file types to the default registry key value list, ".txt, .pdf, .xls, .xlsx, .doc, .docx, .ppt, .pptx" as required.
The permitted file types should have a full stop '.' prefix and should be separated by commas.
A few file types cannot be added to the list of permitted file types and will be ignored if they are added. File types that are not permitted are listed in the File Types that are not Permitted column in the table below.
This table lists the default file types and the file types that are not permitted:
Default File Types File Types that are not Permitted .txt, .pdf, .xls, .xlsx, .doc, .docx, .ppt, .pptx .exe, .pif, .application, .gadget, .msi, .msp, .com, .scr, .hta, .cpl, .msc, .jar, .bat, .cmd, .vb, .vbs, .vbe, .js, .jse, .ws, .wsf, .wsc, .wsh, .ps1, .ps1xml, .ps2, .ps2xml, .psc1, .psc2, .msh, .msh1, .msh2, .mshxml, .msh1xml, .msh2xml, .scf, .lnk, .inf, .reg, .exe, .pif, .application, .gadget, .msi, .msp, .com, .scr, .hta, .cpl, .msc, .jar, .bat, .cmd, .vb, .vbs, .vbe, .js, .jse, .ws, .wsf, .wsc, .wsh, .ps1, .ps1xml, .ps2, .ps2xml, .psc1, .psc2, .msh, .msh1, .msh2, .mshxml, .msh1xml, .msh2xml, .scf, .lnk, .inf, .reg, .apk, .ipa, .sh, .apk, .ipa - Close the Registry Editor.