The Historian does not Contain Data for Certain Points or Accumulators
Historic data is only exported for points and accumulators for which a Wonderware eDNA Historian database item is specified in Export section of the configuration Form. Data that is subsequently stored in the Geo SCADA Expert historian will be exported to the specified Wonderware eDNA Historian servers. For more information about both of these requirements, see Define the Historic Export Details in the Geo SCADA Expert Guide to Core Point Configuration.