Edit an X-Y Plot Item

When you have created an X-Y Plot database item, you need to edit it so that its axes are associated with source data, time line settings are appropriate, and so on. You can use the Edit Trace window to edit the X-Axis, Y-Axis, and Time Line as required.

To edit an X-Y Plot item, you have to be logged on via a User account that has the Configure permission for the item (see Allocating Security Permissions in the Geo SCADA Expert Guide to Security) and is configured to have the Configure Documents and Configure Database settings enabled on the User Form (see User Accounts in the Geo SCADA Expert Guide to Security).

The topics in this section provide information about editing the X-Y Plot components. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2022