Using X-Y Plots

You can use X-Y Plots to view the relationships between data from different sources on a single graphical display. Each X-Y Plot is configured to provide specific data over a specified time period. By accessing an X-Y Plot in Run mode, you can view the data on the plot, and alter the appearance of the X-Y Plot, including altering the time range that is shown.

In this section, we explain how to access an X-Y Plot in Run mode and use its various navigation features. We also describe how to change some aspects of an X-Y Plot’s appearance (for example, how to hide the X-Axis). For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2022