Configure the Font used for the Axis
You can change the appearance of the font that is used for the Time axis text. You do this using fields in the Time Axis Properties window (see Configure the Time-Axis Properties).
Use the Fonts section of the window to specify the font's appearance:
- Font: Use the combo box to select the item of text for which you want to specify the properties. The option is:
- Tick: Select this option to specify the font settings that apply to the text that appears next to the ticks on the selected axis.
- Family: Use the combo box to select the required font family from the list of available fonts.
- Height: Use the spin box to define the size of the text in points. (Point size is the standard term used for font sizes and does not relate to database points.)
- Bold: Select the check box to embolden the text. Emboldened text appears as darker and thicker text.
Clear the check box for the text to retain its normal weight.
- Italic: Select the check box to italicize the text. When italicized, the text slants slightly, typically to the right.
Clear the check box for the text to retain its normal angle.