Change the Appearance of the Dynagraph’s Display

You can change the appearance of a Dynagraph’s display by using the Dynagraph Properties window.


To display the window:

  1. Display the Dynagraph in Design mode (see Displaying an Editor).
  2. Right-click on the main display area of the Dynagraph (the area that will contain the traces).
    A context-sensitive menu is displayed.
  3. Select the Edit Properties option.
    The Dynagraph Properties window is displayed.

Disclaimer

ClearSCADA 2017 R2