Clock Errors

Associated with: DNP3 master outstations

This status attribute indicates whether either of the following has occurred:

Possible States: Displays one of the Standard Alarm States.

(On an outstation on which ClearSCADA does NOT set the clock, the Clock Errors status attribute is ‘Enabled Inactive’, indicating no clock errors.)

Further Information

Outstation Clock.


Disclaimer

ClearSCADA 2017 R2