Communication Statistic Update Properties

Use the fields within the Communication Statistic Updates section of the tab to define how often the communication statistics are updated for the Slave VT Port.

For information on configuring such fields, see Specify the Frequency with which Communications Statistics are Updated.


Disclaimer

ClearSCADA 2017 R2