Configuration Corrupt Alarm

Associated with: DNP3 master outstations

The Configuration Corrupt Alarm attribute indicates whether the outstation’s DNP3 CONFIG_CORRUPT IIN bit is set.

If the bit is set, this indicates that the outstation has detected corrupt configuration. This may relate to the corruption of essential configuration that affects the outstation’s ability to function reliably, or it may relate to non-critical configuration.

An outstation’s CONFIG_CORRUPT IIN bit might be set, for example, when:

Possible States: Displays one of the Standard Alarm States.

See the outstation documentation for information on clearing the CONFIG_CORRUPT IIN bit. Depending on the problem that caused the bit to be set, you may need to re-configure the outstation.


Disclaimer

ClearSCADA 2017 R2