Configure General Point Properties

Use the fields at the top of the <Point Type> tab of the appropriate Point Form to define the general DNP3 settings for a point. Depending on the driver, some or all of these fields may be available. These fields are common to many DNP3 points:


Disclaimer

ClearSCADA 2017 R2