Configure the Counter Reset Method

Use this combo box within the Counters section of the DNP3 tab on the Outstation Form to specify how ClearSCADA resets counters in the outstation:

Reset Method

Use the combo box to specify the required counter reset method. Choose from:

Initialize_DATA (g20v0)

ClearSCADA instructs the outstation to reset the counter value to the default that is specified at the outstation.

WRITE (g20v6) - 16 Bit

ClearSCADA instructs the outstation to reset the counter to a 16-bit value that is specified by the operator. The value is specified using the Initialize pick action.

WRITE (g20v5) - 32 Bit

ClearSCADA instructs the outstation to reset the counter to a 32-bit value that is specified by the operator. The value is specified using the Initialize pick action.


Disclaimer

ClearSCADA 2017 R2