Configure the Outstation Address
Use the Address field at the top of the DNP3 tab to specify the DNP3 address of the outstation.
Each outstation in the ClearSCADA database has to have a unique address. One outstation cannot have the same DNP3 address as another outstation in the ClearSCADA database. Use this field to specify the required address.