Configure the Slave’s Security Properties

Use the fields on the Security tab of each DNP3 Slave Outstation Form to specify properties that relate to DNP3 Secure Authentication when ClearSCADA is operating as a DNP3 Slave.

Use the fields on the Security tab to:


Disclaimer

ClearSCADA 2017 R2