Device Trouble Alarm

Associated with: DNP3 master outstations

The Device Trouble Alarm attribute indicates whether the outstation’s DNP3 DEVICE_TROUBLE IIN bit is set. This bit is typically set when there is a hardware problem at the outstation.

Possible States: Displays one of the Standard Alarm States.

See the outstation documentation for information on clearing the Device Trouble IIN bit.


Disclaimer

ClearSCADA 2017 R2