Enable Unsolicited Alarm

Associated with: DNP3 master outstations

The Enable Unsolicited Alarm attribute indicates whether the DNP3 ‘Enable Unsolicited’ message, sent by the ClearSCADA DNP3 driver to enable unsolicited responses in the outstation, was successful.

The ClearSCADA DNP3 driver will send the ‘Enable Unsolicited’ message if:

Possible States: Displays one of the Standard Alarm States.

Use the Unsolicited Event Reporting Status attribute to determine which unsolicited event classes are enabled in the outstation.


Disclaimer

ClearSCADA 2017 R2