Normal Scan

For outstations for which communications is On Demand or Periodic, see Establishment Scan.

The DNP3 driver can routinely perform various polls—an Integrity Poll, a Class 1 Poll, a Class 2 Poll, a Class 3 Poll, and/or a poll for Static String Point Data. You specify the frequency of each poll using the relevant fields on the Outstation Form.

During an Integrity Poll, the driver requests the outstation to send its Class 1, 2, and 3 event data and Class 0 static (current value) data in chronological order. (The Integrity Polling procedure differs whenever ClearSCADA first establishes communications with a Direct or Shared outstation—see Establishment Scan.)

During a Class Poll, the driver requests the event data for that particular class.

During a String Points Poll, the driver retrieves static (current value) data for string points on an outstation. (String data can also be retrieved using a string point’s Read String pick action.)

An Integrity Poll is typically used to ‘synchronize’ the DNP3 master and slave databases and therefore tends to be assigned a slow poll rate. Class 1, 2, and 3 polls are typically used to retrieve individual class events at varying rates, depending on the importance of those events, with the more critical events being assigned to the classes that have the faster poll rate.

As DNP3 event data is reported by the outstation in chronological order, alarms for the point might raise and clear multiple times during a single poll, as the ClearSCADA server processes each individual event.

Example:

A DNP3 outstation includes this configuration:

Integrity Polling:
Interval:
1D
Offset: Day + 1 Hour

Class 1 Polling:
Interval:
5S
Offset: M

Class 2 Polling:
Interval:
30S
Offset: M

Class 3 Polling:
Interval:
5M
Offset: H

Critical binary events are assigned Class 1.
Important analog events are assigned Class 2.
Other events are assigned Class 3.

With the above setup, ClearSCADA scans the outstation at five-second intervals for Class 1 events, at 30-second intervals for Class 2 events and at five-minute intervals for Class 3 events. Additionally, at 01:00:00.000 each day, ClearSCADA performs an Integrity poll on the outstation.

Some systems depend on outstations sending Unsolicited Messages to report event data to ClearSCADA, rather than on regular polling of those outstations. On such systems, if too much bandwidth is being consumed, consider reducing the rate at which the DNP3 driver polls those outstations for event data.

Further Information

DNP3 Integrity and Data Classes.

Specify When ClearSCADA Performs Integrity Polls.

Specify When ClearSCADA Performs Class Polls.

Specify Whether ClearSCADA Polls an Outstation for Static String Point Data.


Disclaimer

ClearSCADA 2017 R2