Specify how the Driver Determines whether a Reported Value is Out of Range

The Alarm Limits section of the Analog Point tab includes an Out of Range combo box. Use the Out of Range Check combo box to specify how the driver determines whether the point value reported by the outstation is ‘out of range’.

Choose from:

If the driver deems the point value to be ‘out of range’ it processes the value as per the Engineering Units Exceeded setting (see Define how Over Range and Under Range Values are Processed in the ClearSCADA Guide to Core Point Configuration).


Disclaimer

ClearSCADA 2017 R2