DNP Route Table Arguments

When configuring DNP Route Tables, for greatest efficiency enter the most frequently used routes first (one row per route), followed by the less frequently used routes. (The SCADAPack E outstation scans the table entries from top to bottom and stops at the first entry that matches a frame’s destination settings.)

Use these arguments for updating a row in a DNP Route table (for further information and an example of how these arguments might be used, see Route DNP3 Frames Using a DNP Route Table):


Disclaimer

ClearSCADA 2017 R2