Define the Trend Data Sample Type

The fields and options on the Type tab vary, depending on the point on which the outstation is to sample data. Ensure that you Configure the Basic Trend Properties on the Trend tab before configuring the properties on the Type tab.

Use the Trend Type field at the Type tab of the relevant DNP3 SCADAPack E Trend Form to specify the type of point data that the outstation is to sample using this Trend’s settings.

Choose from:


Disclaimer

ClearSCADA 2017 R2