Determine the Restart Level of a Configuration Download

When you use the Download Configuration pick action to perform a configuration download (see Download Configuration) and select the All Configuration option, a Cold Reset is performed. However, if you select the Changed Configuration Only option, ClearSCADA will perform a restart in accordance with the Restart Level of the modified configuration. This level depends on the type of configuration changes that have been made since the configuration was last downloaded to the outstation.

If you need to determine what restart ClearSCADA will issue to a SCADAPack E outstation after a Changed Configuration Only download, generate a temporary version of the configuration file. When you generate the file, ensure that the Full Configuration File check box is clear in the File Options window (see Generate Configuration and Profile Files for Diagnostic Purposes). The Restart Level of the temporary ClearSCADAConfig file will indicate if a Cold Reset will be performed. Depending on the types of configuration changes that have occurred, the restart level will be one of the following:

Further Information

Restart levels that apply to files other than configuration files: see Restart Level.


Disclaimer

ClearSCADA 2017 R2