Reset Download Required Flags
Associated with: DNP3 SACADAPack E outstations and DNP3 SCADAPack Remote E outstations.
Security permission required to access this pick action: Configure.
Use the Reset Download Required Flags pick action to instruct ClearSCADA to clear Configuration Change and Download Required for the outstation, so that the outstation is no longer flagged in ClearSCADA as requiring configuration. Also, if you select this pick action, ClearSCADA will not download existing configuration changes to the outstation if a ClearSCADA operator chooses the Download Configuration pick action with the Changed Configuration Only option set. See Downloading Configuration Changes.