Supported File Types

The types of file that you can download to a SCADAPack E outstation via ClearSCADA include:

In order to import any of these files successfully into ClearSCADA, you need to ensure that the files comply with certain File Restrictions.

Whenever ClearSCADA downloads any RTU Configuration files to a DNP3 SCADAPack E outstation, a log file is added to the list in the Configuration Setup window. You can use this ASCII file for diagnostic purposes (see Configuration Log File).


Disclaimer

ClearSCADA 2017 R2