Use an IP Route Table to Route TCP/IP Packets to Another TCP/IP Host

When a SCADAPack E outstation routes a TCP/IP packet to another TCP/IP host, the following rules are applied in order, until the packet has been sent or discarded:

  1. If only one TCP/IP interface is configured and that interface is PPP, the outstation routes each TCP/IP packet via that interface.
  2. If the TCP/IP packet has a destination address that matches a host on the same subnet as one of the Ethernet interfaces, the outstation routes the TCP/IP packet directly via that ethernet interface.
  3. If the packet has not been sent in step 1 or step 2, above, the outstation looks up the destination address of the packet in the IP Route table. It searches the entries in the route table in Host, Network, Gateway, and finally Default-Gateway order (see Types of IP Route). If a match is found, the outstation routes the packet to the corresponding gateway via the corresponding port.
  4. The packet is discarded.

A SCADAPack E outstation does not differentiate between TCP/IP packets that it generates itself and TCP/IP packets that it receives from another host. It applies the same routing rules to every packet.

If you create and configure an IP Route Table in ClearSCADA, you can use that table to specify up to 20 route entries for outbound TCP/IP packets. You can add entries to the table to allow a SCADAPack E outstation to:

 

Further Information

Types of IP Route.

Add and Configure the Entries in an IP Route Table.


Disclaimer

ClearSCADA 2017 R2