Reset the Filters and Sort Order on a List other than an Alarms List
You can use the Reset Query option to set a List, such as an Events List, Alarm Summary, Queries List, or Historic List to disregard any filtering and sorting that you have applied. This returns the List to its original state—the List will be reset so that it shows the same data as when it was first displayed.
When you first display such a List, ClearSCADA stores the SQL query that specifies which data is shown in the List. As you apply filters and sorting, the SQL Query for the List is altered, but the original SQL Query remains stored in the List document. When you select the Reset Query option, it sets the List to disregard the SQL Query that is currently in place and reinstate the original SQL Query.
To reset a List that is on display:
- Right-click on the List.
A context-sensitive menu is displayed. - Select the Reset Query option.
The SQL Query for the List is reset—any additional filtering and sorting for the List is removed and the List reverts to its original state.
Further Information
Reset the Filters on an Alarms List or the Alarm Banner in the ClearSCADA Guide to Alarms.