NOT

Function Name

NOT

Description

Outputs the opposite value to the input.

Arguments

Input 1 {BOOL}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {BOOL}

If Input 1 is True, the Output is False

If Input 1 is False, the Output is True.

Example:

Function Block Diagram - NOT:

An input named 'FlowPresent' provides a Boolean value. When True, it means that a sensor has detected a flow; when False, the sensor has not detected a flow.

The NOT function returns the opposite value to the input, so if the 'FlowPresent' input is True, the NOT function returns a False value. If the 'FlowPresent' input is False, the NOT function returns a True value.

ST Program - NOT:

The NOT function is used to provide a Boolean value that is True if the input is False, and False if the input is True. The syntax for a NOT function in an ST Program is:

Output := NOT (Input 1);

Where Output and Input 1 are defined as variables earlier in the ST program. Input 1 is a Boolean input and Output is also a Boolean value.


Disclaimer

ClearSCADA 2017 R2