Numerical

Numerical functions allow you to calculate values as absolute values, trigonometric values, natural exponential values, base 10 logarithms, natural logarithms, or square root values. You can also truncate a floating point value into an integer.

You should only use the Numerical functions if you have an understanding of the mathematical principles associated with each of the available functions (the functions are named after a mathematical principle).

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2