Putting it all Together – A ROC Plus Configuration Example
The topics in this section use an example database configuration to demonstrate how you can use the ROC Plus Driver to interface ClearSCADA to a ROC809 flow computer. In the example, the ROC809 is configured to have four stations, with each station having one orifice meter run.
The topics provide information about the example configuration that is contained in a ClearSCADA database export (sde) file, along with information about the various groups and database objects in that example configuration. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.